7/29/2015 10:08 AM | |
Joined: 8/9/2011 Last visit: 11/1/2023 Posts: 324 Rating: (19) |
Hi all, I have (KTP600 basic mono pn) which is already loaded with V11 project. Now I have New CPU (FW V4.0) Loaded with V13 project. (1214C-DC/DC/Rly). Communication is not happening between these two. showing #### on display. I have just changed the Access method to Absolute in HMI tag table and the above said combination is working. But my requirement is i need to communicate the same combination without disturbing HMI . I want to go on CPU side. As discussed in thread there is no option in my TIA Portal (It is a trial version V13) "Permit access with PUT/GET ........" as in attachments.But i find the instructions in instruction tree. can i use it without selecting the option in hardware configuration? Thank you.
---------------------------------------------------------------------------------------------------- |
Last edited by: GaJEnDrA D S at: 7/29/2015 10:11:34 AMLast edited by: Min_Moderator at: 8/3/2015 1:39:17 PMNew subject after splitting "Any intelligent fool can make things bigger, more complex. It takes a touch of genius -- and a lot of courage -- to move in the opposite direction.":):) |
|
4/25/2016 10:19 AM | |
Joined: 8/21/2014 Last visit: 4/24/2024 Posts: 952 Rating: (13) |
New question published by 9583815919 is split to a separate thread with the subject Communicating with KTP600 using TIA Portal. Best regards |
My Forum is the place to personalize your profile, |
|
10/1/2018 6:40 PM | |
Posts: 1 Rating: (0) |
KTP600 and TIA V13 no communicationi am facing same problem with my machine. s7 1200 4.0 with old ktp600. No communication. ### Can you give details , how you sloved your problem. thanks in advance |
Follow us on