8/3/2015 3:26 PM | |
Posts: 3093 Rating: (322) |
Hello Ariel, Regards, |
8/10/2015 8:55 PM | |
Posts: 439 Rating: (108) |
Ariel, Here is an archived project (Project and Retrieve) of two S7-1200 communicating in Modbus, one is Modbus server and the other is Modbus client. I am pretty sure it is the same block and method to use the block between S7-1200 and S7-1500. https://www.dropbox.com/s/80513eaofg30dod/Modbus%20TCP%20V4%20S7-1200%20OK.zap13?dl=0 This is a TIA Portal V13 SP1 update 4 project. I hope this will help you. Best regards, Hugo |
This contribution was helpful to1 thankful Users |
Follow us on