9/3/2015 10:57 AM | |
Posts: 4 Rating: (0) |
Hi, I have changed the gear from 2 step gear (ratio 14,901 and 3,031) to one single gear (ratio 7,79) Theres is a motor encoder(0) and an encoder(1) mounted on the gear I changed parameters: 31050=from 1000 to 100 31060=from 14901 and 30310 to 779 The gear change is disabled and always in gear 1. When positioning the spindle everything works correctly, both encoders count similar to the set position. The problem is when using M3 or M4 speed mode, i get a user alarm"700114 Spindle -Motor/Spindle is different" programmed by the machine manufacturer that i cannot trace because of locked plc. The alarm occurs after about 1 second no matter what speed is programmed. Is there any other parameters to be changed for this to work properly ? Update: When following error is greater than 1 - the alarm occurs, below 1 everything is ok. Spindle MD attached Alexander AttachmentMD SPINDEL VDF ORIG.txt (152 Downloads) |
Last edited by: Frankimonn at: 9/3/2015 12:14:38 PMLast edited by: Frankimonn at: 9/3/2015 3:26:32 PMLast edited by: Frankimonn at: 9/3/2015 3:29:18 PM |
|
9/3/2015 11:37 AM | |
Joined: 1/19/2008 Last visit: 4/19/2024 Posts: 980 Rating: (63) |
Hi, Maybe you would like share the alarm text ? Pee |
9/3/2015 11:56 AM | |
Posts: 4 Rating: (0) |
Yes, that may be helpful ! 700114 Spindle -Motor/Spindle is different |
Follow us on