10/6/2015 11:02 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1051) |
hi aney, the CPU has a power-supply for it self, and it is running the backplane-bus. The electronic-modules maybe need a power supply too, but this is coming from the Base-Units. Therefore the first BU has to be a light one, because the ligth BU is opening a new potential group. It is recommented to use the TIA Selection Tool to project the systems. It is a free software to select all needed components. hope this helps, regards, |
FCK WAR! |
|
This contribution was helpful to1 thankful Users |
10/8/2015 11:09 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1051) |
yes, you´re right. regards |
FCK WAR! |
|
This contribution was helpful to2 thankful Users |
Follow us on