10/5/2015 12:37 PM | |
Joined: 12/18/2014 Last visit: 9/19/2024 Posts: 33793 Rating: (4197) |
Expect really anyone can comment on it without knowing your program? Please Upload your program. |
10/5/2015 7:03 PM | |
Posts: 49 Rating: (5) |
Here's the program. AttachmentCounterDataLog-Upload.zip (203 Downloads) |
10/5/2015 7:07 PM | |
Posts: 49 Rating: (5) |
Here's segment of the Data file that's uploaded. Another weird thing. At row 6 when the counter get reset to zero (Log triggered when I5 is triggered, so 1st register will be 1 and not zero), the CSV for the Inputs 1 to 8 become null instead of zero. ---------------------------------------------------- Time,B001.Cnt ,B003.AQ,B007.Cnt ,B006.Cnt ,B019.Cnt ,B021.AQ,B013.CurT,I1,I2,I3,I4,I5,I6,I7,I8 5/10/2015 17:19,89,437,1819,13112,89,189,433,0,0,0,0,0,0,0,0 5/10/2015 17:22,90,437,1820,13113,90,189,410,0,0,0,0,0,0,0,0 5/10/2015 17:25,91,437,1821,13114,91,189,313,0,0,0,0,0,0,0,0 5/10/2015 17:27,92,437,1822,13115,92,189,217,0,0,0,0,0,0,0,0 5/10/2015 17:33,1,0,1,1,1,0,209,0,,,,,,, 5/10/2015 17:38,2,0,2,2,2,0,110,0,,,,,,, 5/10/2015 17:44,1,0,1,1,1,0,342,0,,,,,,, 5/10/2015 17:51,2,0,2,2,2,0,268,0,,,,,,, Attachmentuploadcsvtest.xlsx (185 Downloads) |
10/5/2015 7:55 PM | |
Joined: 12/18/2014 Last visit: 9/19/2024 Posts: 33793 Rating: (4197) |
The logo is not a PLC, it's an logic module. Says Siemens. |
Follow us on