10/2/2015 7:24 PM | |
Posts: 12 Rating: (0) |
Dear Mr we have a machining center with numerical control Siemens 810 M, I would like to transfer data from PC to the machine by using an RS 232 cable, what software I need to install it on my PC to communicate with it. the machine is panne, when i push in the key T17 to start CN , but does not change anything, the machine remains at rest without display any alarm CN, PLC. i have an archive that contains the PM machine (CN, PLC interface) and the PLC programme can you help me how to load the PLC programm from Pc and to read it in MDI mode in machine Best regard ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 10/5/2015 10:45:02 AMNew subject after splitting |
|
10/6/2015 12:13 AM | |
Joined: 10/17/2007 Last visit: 9/17/2024 Posts: 4031 Rating: (353) |
@aymen1985 Hi, Friend , Min_Moderator transfer your post from S5 to HERE SINUMERIK, I am know 810M very well ,as well as SINUMERIK 840D OR 810D, I need you make clean, what system you have 810M, what version such as GA3 OR GA1.check Siemens part# on the back of controller to get it.Then I and other can help you better and I am confused by you description: what is T17, what kind of file do you want transfer--only PLC program? or more. You can add more information, such as what kind of PC you have ( better Laptop) , OS--WinXP is best, also you can search in this forum--key word "transfer file to SINUMERIK 810M" I REMEMBER FOR 2 OR 3 YEARS ,THERE ARE SOME VERY GOOD POST for that topic.
|
If you like my comments please |
|
Follow us on