10/5/2015 7:39 PM | |
Joined: 12/18/2014 Last visit: 5/11/2024 Posts: 33009 Rating: (4079) |
Look at attachment.
AttachmentLOGO! Soft manual 0BA7 english side 286.pdf (173 Downloads) |
10/5/2015 9:00 PM | |
Posts: 158 Rating: (1) |
Hi, thank you! Attached is the file I'm referring to. I highlighted all the 'on' states, and and the "I" columns at the top that are, or could be, maintained inputs (like a limit switch). I don't understand, how, if the EN signal is ON and prevents other datalog writes, are there multiple rows at different times? I will upload the code itself next. It's part of a larger program I stripped off, but this is all that pertains. Attachment205_6.pdf (192 Downloads) |
10/5/2015 9:03 PM | |
Posts: 158 Rating: (1) |
here's the code that generated the data logAttachment712MSRUDLONLY.pdf (210 Downloads) |
Follow us on