4/25/2013 6:43 PM | |
Posts: 2 Rating: (0) |
Hello everybody, Firts of all, I hope to be in the right sub-forum. I'm having a small problem. My Comprofibus v5.1+SP1 is not "accepting" some .gsd files. I put them in the library of Comprofibus, file-> read in new .gsd but nothing. I've attached 1 of the .gsd files. In Step7 they seem OK (says my co-worker). Unfortunately I've zer experience with Step7. Thanks in advance. Stijn. AttachmentSMCB1411.pdf (333 Downloads) |
4/26/2013 5:29 AM | |
Joined: 8/25/2006 Last visit: 9/20/2024 Posts: 2209 Rating: (278) |
Hello. I try your gsd-file on ComProfibus V5.1.2.3, it is recognized ok (look at screenshot). So try to upgrade ComProfibus to the latest version V5.1 SP2 HF3: and after installHotfix 3 for COM PROFIBUS V5.1
|
This contribution was helpful to1 thankful Users |
4/26/2013 12:19 PM | |
Posts: 2 Rating: (0) |
Hello, the problem is solved. Thank you for helping me out. (Thread can be closed) Kind regards, Stijn. |
11/19/2015 4:36 PM | |
Joined: 3/5/2015 Last visit: 7/29/2024 Posts: 1 Rating: (0) |
Hello, I've installed these 2 hotfixes but I am still unable to load certain gsd files. Please have a look at the attached gsd file. Thank you Attachmentgsd.zip (263 Downloads) |
11/20/2015 5:21 AM | |
Joined: 8/25/2006 Last visit: 9/20/2024 Posts: 2209 Rating: (278) |
Hello. On my PC your gsd-file is recognized without problem. Look at screenshot. |
Follow us on