9/18/2015 12:23 PM | |
Joined: 9/15/2015 Last visit: 10/5/2023 Posts: 3 Rating: (0) |
Hello everybody! I'm trying to set communication with my S200 using option 3. USBinterface6GK1571-0BA00-0AA0. I stuck on information "Specifed acces point not found". Can someone explain me what is wrong with that? In box "Acces point of the application" attached in PG/PC interference I have 4 options: 1. _CP_L2_1 2. FWL_LOAD 3.MPI (WIN_CC) 4.S7ONLINE Nothing works properly. It looks like something is missing here. I will be very appreciate for any kind of help! If it's important I work on windows 7 service pack 1. Edit: Now I've found the following manual to my adapter. I'm not sure it's going to work with my s200. Can someone resolve my doubts?
------------------------------------------------------------------------------------------ |
Last edited by: nobodyyyx at: 9/18/2015 12:35:47 PMLast edited by: nobodyyyx at: 9/18/2015 12:37:46 PMLast edited by: CS Moderator at: 9/18/2015 2:35:35 PMNew subject after splitting |
|
11/10/2015 1:18 PM | |
Joined: 10/22/2015 Last visit: 12/18/2022 Posts: 4 Rating: (0) |
Hi, Did you solved your problem? I have same troubles... |
Everything is possible it just needs more time |
|
11/10/2015 2:43 PM | |
Joined: 1/21/2013 Last visit: 9/4/2024 Posts: 4620 Rating: (707) |
Hello, Should work, how is your setting in PG/PC interface? Manual wrote: The PPI bus profile can be used via the "Universal" PROFIBUS bus profile |
11/23/2015 2:53 PM | |
Joined: 4/28/2015 Last visit: 2/7/2024 Posts: 10533 Rating: (820) |
Hello, if your interface is missing from list, use this patch. It can show Microwin option too, if it wasn't there. Edit: look at batch file manually, if your directories doesn't correspond with batch, try find that exe on disk and run it with that parameter manually. AttachmentPCPPIcable.zip (513 Downloads) |
Last edited by: Duris_I at: 11/23/2015 5:25:42 PMWith best regards... |
|
Follow us on