11/28/2015 12:47 PM | |
Joined: 5/20/2015 Last visit: 4/24/2024 Posts: 216 Rating: (3) |
HELLO FRIENDS, I TOO HAVE A SAME TROUBLE, INFACT I HAVE DEVELOPED AN INTEGRATED PROJECT OF TWO S7-1214C DC/DC/DC CPUs, THING IS THAT THERE IS NO COMMUNICATION AND CONFIGURATION PROBLEM , BUT STILL I AM NOT GETTING OUTPUTS WHEN REQ TO GET OR PUT BLOCKS IT DOES NOT RESPONSE WITH ANY ERROR THATS WHY IT IS DIFFCULT TO DIAGNOSE AND TROUBLESHOOT. MY APPLICATION IS JUST LIKE SYNCRONIASTION BETWEEN TWO DUPLICATE CPUs, AS YOU SAID USE MOVE BLOCK INSTRUCTION TO GET IT DONE. SO PLEASE COULD ANYONE CAN PROVIDE ME A SAMPLE PROGRAM OF SUCH RELEVENT APPLICATION. PLEASE SOMEBODY HELP ME. THANK YOU, ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 11/30/2015 10:10:37 AMNew subject after splitting Let's do it... |
|
11/30/2015 10:11 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4774 Rating: (123) |
|
This contribution was helpful to1 thankful Users |
Follow us on