12/31/2015 5:06 PM | |
Joined: 3/21/2006 Last visit: 4/4/2024 Posts: 10228 Rating: (1181) |
https://support.industry.siemens.com/cs/ww/en/view/113498 look there for Station type: ET 200M (IM153-2 High Feature) DPV1, H, 12 I/O Order no.: 6ES7 153-2BA*0-0XB0Version: V6.0 (01/2015) |
This contribution was helpful to1 thankful Users |
12/31/2015 5:13 PM | |
Joined: 5/12/2006 Last visit: 4/23/2024 Posts: 22224 Rating: (2979) |
Hello, from the Manual of the Interfacemodule: When configuring the DP/PA Link with GSD tool: You must select the predecessor "2BA82". The GSD tool is available for download free-ofcharge on the Internet (http://support.automation.siemens.com/WW/view/en/26562190).
Christoph |
This contribution was helpful to1 thankful Users |
12/31/2015 5:14 PM | |
Joined: 12/22/2006 Last visit: 1/25/2022 Posts: 1742 Rating: (306) |
Hello, In this product note: https://support.industry.siemens.com/cs/us/en/view/109475772, there is a statement Configuration information
Means to me that you can use the 6ES7153-2BA82-0XB0 as substitute for the new module. Hope an expert can confirm that.
The very first topic is: |
Last edited by: jklm at: 12/31/2015 5:15:45 PMLast edited by: jklm at: 12/31/2015 5:22:23 PMBest regards |
|
This contribution was helpful to1 thankful Users |
12/31/2015 5:25 PM | |
Posts: 10 Rating: (0) |
hi, I installed IM153-2BAx0_HF_DPV1_H_12IO gsd file at hardware. but it is only ET-200M. It don't display in DP/PA link , so i can't configure for Y-link. |
12/31/2015 7:59 PM | |
Joined: 3/21/2006 Last visit: 4/4/2024 Posts: 10228 Rating: (1181) |
https://support.industry.siemens.com/cs/ww/en/view/51678187 |
2/7/2016 9:32 AM | |
Joined: 9/2/2012 Last visit: 4/18/2024 Posts: 711 Rating: (30) |
Hi, It's solved... Not yet
|
Last edited by: vipz at: 2/19/2016 7:24:16 PM
|
|
Follow us on