2/12/2016 9:56 AM | ||
Joined: 4/2/2015 Last visit: 12/26/2023 Posts: 5 Rating: (0) |
Dear Mr. Ste39,
One of our customer is trying to hook up a SCHENCK PROCESS Make Weigh Feeder to our S7-400 CPU over PROFIBUS.
Wit the GSD file given by the manufacturer, there is some firmware mismatch with respect to our S7-400 CPU. Details of our CPU and the Schenck weigh feeder is as below:
1.Intecont-tersus(VEG20650) -VPB 28020 profibus-dp interface card is available with customer. Need your support in getting the right GSD file. REgards Sree
------------------------------------------------------------------------------------------ |
|
Last edited by: Min_Moderator at: 2/12/2016 10:41:20 AMNew subject after splitting |
||
2/12/2016 6:49 PM | |
Joined: 9/27/2006 Last visit: 9/19/2024 Posts: 12282 Rating: (2684) |
Hello anansree;7 Manufacturers of Profibus slaves are responsible for the creation and distribution of the gsd files for their equipment. For such an enquiry, and since the Schenck site does not provide much information on the subject, I believe that the best resource would be to contact Schenck Process directly. See their site: http://www.schenckamericas.com/contact.html Hope this helps, Daniel Chartier |
This contribution was helpful to1 thankful Users |
2/24/2022 4:04 AM | |
Joined: 5/21/2009 Last visit: 7/30/2024 Posts: 4 Rating: (0) |
hi, found all the gsd file here (from schnenk web site): |
This contribution was helpful to1 thankful Users |
Follow us on