2/4/2016 5:02 PM | |
Joined: 5/28/2010 Last visit: 3/25/2019 Posts: 17 Rating: (0) |
Hi everybody I have a problem with picture module(in Dynamic wizard). According to attached file I create a picture module instance that connected to a Structure Tag with name "com". I want to have an I/O filed that when I press each buttons the value of I/O field change. But in runtime when i press vary button I/O field that placed in picture module template changed but correspond external I/O field did't change. The other note that must point is that when I change I/O field in picture module(in runtime in main.pdl) and press "ENTER" key external tage change fine I think I need to create "ENTER" key automatically when I/O field change. But I don't know exactlly who can I do it. my wincc version is wincc v6sp4 I place wincc and simatic program in help.zip Best Regards Attachmenthelp.zip (132 Downloads) |
2/18/2016 6:45 AM | |
Joined: 5/28/2010 Last visit: 3/25/2019 Posts: 17 Rating: (0) |
Hi HarrY ji I did what I suppose to do with new method. I use text list and it work very fine. I send that file for you to see. but I was so enthusiastic to do my job with previous method. By the way thanks for reply. if you had any suggestion for me about that job please send me your idea Best Regards AttachmentTEST2.zip (171 Downloads) |
Follow us on