5/3/2016 5:46 PM | |
Posts: 13 Rating: (0) |
Hello LesPaul, I am facing an issue with a Positioner-1 configuration in Simocode pro v. Whenever the positioner is at OPEN condition and then if the CLOSE command is given, the End Position fault appears in Simocode almost instantly. So, how can I rectify this? Also, is there any way to disable this fault from appearing ? Thanks, Anuj ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 5/4/2016 11:02:39 AMNew subject after splitting |
|
5/4/2016 7:07 PM | |
Posts: 13 Rating: (0) |
(1) The fault appears in both cases, that is, the command pulse is long or short (2) The end position limits have been wired to the Digital Module-1 Regards, Anuj |
Follow us on