5/4/2016 7:53 AM | |
Joined: 4/20/2016 Last visit: 3/20/2023 Posts: 4 Rating:
|
Dear Sir I am using s7-315 2pn/dp , 2 IM-153-1 and 153-8 communication with profiibus , I want to try profibus communication 1.5mbps , problem is plc go to bus fault and system fault ,and now i set 1.87mbps then communication is ok but after 5 minute communication breack , i want to know what is problem, profibus rang is 4 to 5 meter ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 5/4/2016 12:01:35 PMNew subject after splitting |
|
5/11/2016 9:41 PM | |
Posts: 163 Rating:
|
Hello, I have the same problem as this guy, my cable length is just 30 or 40 cm. Is that problematic? |
5/11/2016 11:15 PM | |
Joined: 9/27/2006 Last visit: 7/31/2024 Posts: 12272 Rating:
|
Hello ldir; There was a recent discussion on this issue recently: Bus fault in profibus network https://support.industry.siemens.com/tf/ww/en/posts/100984/ In one of the posts you will find a link to the official introduction of the so-called "1 meter rule" for Profibus networks in the Profibus International guides for Profibus-DP installations. Basically, the 1 meter rule officialises what expert Profibus network designers knew from experience, that a length of less than a meter of copper cable between 2 nodes will lead to reflexions on the line and introduce errors of data transmission. And no diagnostics are available in Profibus masters to detect that type of error, outside of oscilloscope analysis of the signal, which not everyone is capable of interpreting correctly (recent experiences have shown that I personally am quite deficient in that type of debugging). If you have less than a meter of cable between the nodes, you should thinkl of replacing you cable with one-meter (or more) lengths. Hope this helps, Daniel Chartier Edit: you will find in attachment the official text on the 1 meter rule from this official document PROFIBUS_Assembling_8022_V114_May15.pdf that you can download from Profibus.com: http://www.profibus.com/download/installation-guide/ Even though they have inserted conditions on the type of connector used, most experienced installers will always apply the 1m rule when designing a Profibus installation. D.C. |
Last edited by: dchartier at: 5/12/2016 12:35:59 AM |
|
This contribution was helpful to
1 thankful Users |
5/12/2016 3:16 PM | |
Joined: 7/22/2008 Last visit: 4/14/2022 Posts: 1884 Rating:
|
RIP |
Last edited by: 1test at: 6/8/2016 9:12:58 AM~(‾▿‾)~ |
|
5/12/2016 5:16 PM | |
Posts: 163 Rating:
|
Thanks but i dont have that CP card. |
Follow us on