5/26/2016 8:00 PM | |
Joined: 2/1/2010 Last visit: 5/10/2024 Posts: 136 Rating: (68) |
I think you must be using Drive ES PCS7 (Classic). Have you ensured you have the correct version installed? You can check this page: https://support.industry.siemens.com/cs/document/109474976/drive-es-pcs7-v8-1-sales-and-delivery-release-(classic-style)?dti=0&lc=en-US Also note that some G120 drives need a different block based on hardware revision. |
If my post helped you, please rate. Thanks. |
|
This contribution was helpful to1 thankful Users |
5/31/2016 7:52 PM | |
Joined: 1/15/2009 Last visit: 4/19/2024 Posts: 316 Rating: (40)
|
Was the project originally created on this Engineering Station or another? If another, can you compare the 'Installed Software' files from the two to verify the library installations are the same (specifically around Drive ES for PCS 7) Was this an upgrade? Then perhaps like RVSwick mentions, you may not have updated the Drive ES library along with the PCS 7 version... see the compatibility tool for the correct versions of PCS 7 and the other software installations https://support.industry.siemens.com/kompatool/pages/main/index.jsf |
The best location for all PCS 7 content (manuals, guides, application notes, FAQs, and videos). |
|
This contribution was helpful to1 thankful Users |
Follow us on