7/24/2016 10:49 AM | |
Posts: 2 Rating: (0) |
Recently i have installed Wincc Flexible 2008 SP2 and tried to open a previously completed project but couldn't succeed and it says that "the project was created with an incompatible or beta version of wincc flexible..." Here i have attached two images for getting an idea regarding the error massage and installed version of my Wincc Flexible. Thanks in advance for your suggestions. AttachmentImage.zip (108 Downloads) |
Last edited by: Aminul at: 7/24/2016 11:08:16 AM |
|
7/24/2016 11:11 AM | |
Joined: 1/21/2013 Last visit: 9/4/2024 Posts: 4620 Rating: (707) |
Hello, Many thread with this problem, check above on right beside Site Explorer and search: one thread: https://support.industry.siemens.com/tf/WW/en/posts/bypost/?postId=238770 |
This contribution was helpful to1 thankful Users |
7/24/2016 11:28 AM | |
Posts: 2 Rating: (0) |
Thanks for your reply. Could you please let me know which one will work for me Latest update of Wincc Flexible 2008 SP2 or Wincc Flexible SP3 if it is SP3, how to upgrade from SP2 to SP3. Thanks |
7/24/2016 11:39 AM | |
Joined: 1/21/2013 Last visit: 9/4/2024 Posts: 4620 Rating: (707) |
Hello, Sorry now no have a PC i can't download your Zip file but have a look this: |
Last edited by: Ste39 at: 7/24/2016 11:40:16 AM |
|
7/25/2016 1:17 PM | |
Joined: 8/3/2009 Last visit: 9/23/2024 Posts: 13759 Rating: (1738)
|
Hello Aminul The meaning of the V1.4 Upd5 is WinCC flexible 2008 S3 Up5. So you cannot open a newer Project with an older version. So you do not need a new License for SP3 but you have to install it. Here you can download it. With your license its a full version: https://support.industry.siemens.com/cs/ww/en/view/100777999 then install the latest update out of the Last post. Then you should be able to open the Project. Bye Murof |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to1 thankful Users |
Follow us on