7/19/2013 11:16 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
Please refer the attached sheet. DC DC link over voltage LED lits on. Check your incoming supply voltage & DP switch setting on the infeed module.Please refer the attched sheets for more information.If the supply voltage is within acceptable limit, observe when this LED lits? i.e. during stoping of main spindle?(I assume as main spindle is driven by 611 drive) Please check & revert back. AttachmentInfeed module LED significance.zip (1802 Downloads) |
This contribution was helpful to2 thankful Users |
7/18/2016 3:02 PM | |
Posts: 1 Rating: (0) |
Hello I have same problem in simodrive DC link voltage goes upto 700 and alarm comes dip switch s1.1 is on please let me know if any solution
|
1/22/2022 11:33 AM | |
Posts: 1 Rating: (0) |
YOU NEED TO CHECK LOSS POWER CONNECTION |
Follow us on