8/19/2016 5:20 AM | |
Posts: 3 Rating: (0) |
We faced a CPU error yesterday, and error information, please see the attachment. When the fault happened, the equipments were still running, the "stop" lamp flash. We push "reset" button to reset, no function. So we downloaded the program to CPU, the CPU worked well. Could anyone give me a hint how to analyse these errors and how to solve it. And what does "Log. base address of the DP slave: Input address: 16294 Log. base address of the DP master: 16201" mean? Thanks. AttachmentDiagnose0817 (2).txt (328 Downloads) |
Follow us on