8/17/2016 2:52 PM | |
Posts: 4 Rating: (1) |
Hello I am using Simatic Manager V 5.5. The problem is as follows There is SF error and BF error. In Profibus there are 32 connected devices. Out of 32 there are 9 IM 151 (IO) and rest 23 are inverter (Micromaster 420). All profibus connector are checked and terminaotor on first and last device is on. I should mention that, first and last device is IM 151. In online condition all inverters are disconnected and all IM 151 is connected. In module information it shows the status as "Inverter.jpg" of station no 36. For this reason i tried to reconfigure the hardware for inverter. Now i am able to add MICROMASTER 4 from PROFIBUS DP > SIMOVERT, after deleting profibus device id no 36 as picture "Inverte Replace.jpg". But during save and compile it shows the message as picture "SaveCompile.jpg". All three pictures are inserted in attached "Inverter.doc" file. Warm Regards mafizurtutul
AttachmentInverter.doc (415 Downloads) |
10/18/2016 4:53 AM | |
Posts: 1 Rating: (0) |
hi can u tell me how u fixed your faul?i got same problem |
Last edited by: 03152 at: 10/18/2016 4:53:36 AM |
|
3/4/2019 9:28 AM | |
Posts: 1 Rating: (0) |
HI. CAN U TELL ME HOW U FIXED IT? I GOT THE SAME PROBLEM! |
Follow us on