12/24/2014 5:44 AM | |
Posts: 15 Rating: (0) |
Good Morning, I have some problem with coomunication between only one S7-400 (of 12) and WinCC. Loss of communication occurs in different time, duration about 5 sec. SIMATIC_S7_Protocol_Suite_01.LOG: 2014-12-11 08:48:34,975 ERROR Connectionerror 2169 "GPA2_GPA2": Errorcode 0x0000 7002! 2014-12-11 08:51:52,738 ERROR Connectionerror 2170 "GPA2_GPA2": Errorcode 0x0000 7002! 2014-12-11 08:54:04,108 ERROR Connectionerror 2171 "GPA2_GPA2": Errorcode 0x0000 7002! 2014-12-11 08:57:25,473 ERROR Connectionerror 2172 "GPA2_GPA2": Errorcode 0x0000 7002! 2014-12-11 10:15:21,119 ERROR Connectionerror 2173 "GPA2_GPA2": Errorcode 0x0000 7002! 2014-12-11 12:57:38,544 ERROR Connectionerror 2174 "GPA2_GPA2": Errorcode 0x0000 7002! 2014-12-11 13:11:04,121 ERROR Connectionerror 2175 "GPA2_GPA2": Errorcode 0x0000 7002! 2014-12-11 15:09:50,446 ERROR Connectionerror 2176 "GPA2_GPA2": Errorcode 0x0000 7002! 2014-12-11 16:01:23,668 ERROR Connectionerror 2177 "GPA2_GPA2": Errorcode 0x0000 7002! 2014-12-11 18:00:16,871 ERROR Connectionerror 2178 "GPA2_GPA2": Errorcode 0x0000 7002! 2014-12-11 20:21:03,222 ERROR Connectionerror 2179 "GPA2_GPA2": Errorcode 0x0000 7002! 2014-12-11 20:22:57,884 ERROR Connectionerror 2180 "GPA2_GPA2": Errorcode 0x0000 7002! 2014-12-11 20:28:58,243 ERROR Connectionerror 2181 "GPA2_GPA2": Errorcode 0x0000 7002! 2014-12-11 20:31:42,046 ERROR Connectionerror 2182 "GPA2_GPA2": Errorcode 0x0000 7002! 2014-12-11 20:49:12,229 ERROR Connectionerror 2183 "GPA2_GPA2": Errorcode 0x0000 7002! 2014-12-11 20:58:40,894 ERROR Connectionerror 2184 "GPA2_GPA2": Errorcode 0xFFDF 410E! 2014-12-11 21:03:24,430 ERROR Connectionerror 2185 "GPA2_GPA2": Errorcode 0x0000 7002! 2014-12-11 21:15:08,773 ERROR Connectionerror 2186 "GPA2_GPA2": Errorcode 0x0000 7002! 2014-12-15 11:14:11,731 ERROR Connectionerror 2187 "GPA2_GPA2": Errorcode 0x0000 7002! 2014-12-21 18:22:24,832 ERROR Connectionerror 2188 "GPA2_GPA2": Errorcode 0x0000 7002! Ping GPA2 - ok in all time. Can you help me? Regards, Dmitriy AttachmentPrtScn.zip (103 Downloads) |
12/30/2014 1:11 PM | |
Posts: 15 Rating: (0) |
Hello,bg2492! Many thanks for you kind feednack. I will try it later. Best regards.
|
Follow us on