8/25/2016 5:53 PM | |
Joined: 9/27/2006 Last visit: 4/23/2024 Posts: 12257 Rating: (2665)
|
Hello Vlad; To be able to provide you out with more detailed information, we need to know the exact part number of the CPU you are using. Here, as an example, I have a link to the firmware upgrades of the 6ES7 314-6EH04-0AB0 CPU: Operating System Updates for CPU314C-2PN/DP (6ES7314-6EH04-0AB0) https://support.industry.siemens.com/cs/fr/en/view/51466769 Even if this is not the part number you have, please read the accompanying information: there are elements here that apply to all upgrades. -it is recommended to always upgrade to the latest version possible; -unfortunately, upgrading the firmware requires you purchase a MMC (8MB). Hope this helps, Daniel Chartier |
8/26/2016 9:37 AM | |
Posts: 4 Rating: (0) |
CPU is 6ES7-314-6CF00-0AB0 with firmware 1.03. I have seen 1.05 but there is no major changes listed regarding this issue directly. Since it first generation it can be upgraded via MMC. But we do not have an PROM adapter is there possibilities to buy MMC with OS upgrade for this PLC? I am not sure if it helps anyway as I mentioned I don't see workarounds for this CPU and CP 343 compatibility. |
Follow us on