8/30/2016 9:07 AM | |
Joined: 2/4/2015 Last visit: 7/26/2023 Posts: 64 Rating: (0) |
Hi all, I have made Siemens PLC test setup with the following configuration but CPU is not going in Run mode after downloading hardware configuration. Without any IM CPU is going online. Kindly help me out. CPU is 416-5H I am having a doubt whether redundant CPU and redundant IM can be used in a non redundant configuration or not. Regards Surendhar M ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 8/30/2016 3:31:23 PMNew subject after splitting Last edited by: Min_Moderator at: 8/30/2016 3:32:02 PMContact data removed |
|
Follow us on