8/31/2016 5:58 PM | |
Posts: 2 Rating: (0) |
Hello I have connecting two cpu 313c-2DP with a cable profibus, the PC adapter (MPI) is connected with a master CPU but i have an error (SF and BF are RED). In the partners accesible I show just the CPU master My cable profibus is on mode on in the two sens see attachment ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 9/1/2016 8:33:12 AMNew subject after splitting |
|
9/8/2016 12:11 PM | |
Posts: 2 Rating: (0) |
I need a document of how i configure tow CPU S7-300-2DP, slave master profibus dp with TIA PORTAL v12or v13. Thanks |
9/8/2016 1:34 PM | |
Joined: 4/28/2015 Last visit: 2/7/2024 Posts: 10533 Rating: (818) |
Hello, look, some topics under this one you can probably find your answer, only put some energy to this. Profibus between cpu1516 3PN/DP and cpu315-2dp |
With best regards... |
|
9/8/2016 2:07 PM | |
Joined: 9/27/2006 Last visit: 4/24/2024 Posts: 12257 Rating: (2665) |
Hello: Here are a few more links, not perfect by themselves, but the should be helpfu: - a step-buy-step video tutorial on S7-300 maser-slave over Profibus-DP, with TIA Portal (well-done, in Spanish); https://www.youtube.)com/watch?v=ciTbYIYs0LI - a manual on Profibus-DP configurations with TIA Portal, with examples based on the S7-1500 SIMATIC PROFIBUS PROFIBUS with STEP 7 V13 https://support.industry.siemens.com/cs/fr/en/view/59193579 Hope this helps, Daniel chartier |
This contribution was helpful to1 thankful Users |
Follow us on