2/26/2007 1:14 AM | |
Posts: 1 Rating: (0) |
Hi, can anyone please help me with the TECHNICAL details of motor type 1LA8 453-6PS50-Z450 |
3/1/2007 7:22 AM | |
Joined: 10/11/2006 Last visit: 9/18/2024 Posts: 5906 Rating: (804)
|
Hello Raja, -z means special options, but I can't find an option 450. Can you please check wether -z 450 is right or not? Maybe there are some more options.If you have the serialnumber of the motor you can open a service request for this question at support.automation@siemens.com and they can check the options with the serialnumber. The1LA8453-6PS50 without optionis: LOW-VOLTG. SQUIRREL-CAGE MOTOR IP 55, WITH SPECIAL ROTOR FOR SIMOVERT MASTERDRIVES OPERATION TEMP. CLASS F, 6 PTC THERMIST. 6-POLE, 630KW, 50HZ (MAINS) * SIZE 450 3 AC 50HZ 500VD IM B 3 But take care, maybe with the options, the electrical data may be different! Best regards Tech Team |
With best regards, |
|
9/22/2016 4:47 PM | |
Posts: 767 Rating: (69) |
Good Morning Would you please send us the winding information and diagram for a motor 1LA8 403-4AB90-Z S/N A-31290659010001 / 2010 D-90441 NURNBERG |
Follow us on