10/24/2016 9:38 PM | |
Joined: 12/1/2009 Last visit: 3/31/2024 Posts: 672 Rating: (147) |
HelloAhooraJafari, S5 is history. However, you should consider using an external device/controller with I/O and connect it to your S5. There are small compact devices with limited number of I/O sending SMS,email or whatsever and can receive commands to control outputs. I believe such device will do the job The below is just an example in order to push you in the right direction: http://www.siemens.se/bu/as/insta/doc/beta_produktinformation_gsm-larmmodul5tt7.pdf Best Regards. |
Give us your feedback and show us your respect! |
|
This contribution was helpful to3 thankful Users |
10/25/2016 9:26 AM | |
Joined: 3/27/2012 Last visit: 3/7/2024 Posts: 179 Rating: (4) |
Thanks TIBI68 |
This contribution was helpful to2 thankful Users |
Follow us on