2/27/2017 4:10 PM | |
Joined: 4/28/2015 Last visit: 9/9/2024 Posts: 3345 Rating: (379)
|
Hi JDarius,
I attached an example which uses the IOT2000 time as timestamp. If you synchronize your PLC and your IOT with the same ntp server, this should be a good way.
Yes this would trigger every second, if the timestamp format changes every second.
S7 connection is no problem with PLCSim Advanced. So this should work, but I have to check this too.
Do you have connection to your PLCSim Advanced? Ping is possible? If not make sure that you selected "Virtual Ethernet Adapter" in your PLCSim settings. Are there some errors displayed by node-red? AttachmentData+Timestamp.txt (1649 Downloads) |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
Follow us on