3/1/2017 2:23 PM | |
Joined: 5/12/2006 Last visit: 9/18/2024 Posts: 22364 Rating: (3011)
|
Hello, can you attach the project here? Christoph |
3/1/2017 2:41 PM | |
Joined: 3/9/2015 Last visit: 9/19/2024 Posts: 17 Rating: (0) |
We have strict IP rules at our company I can't publish the project here. But check out my previous post, I think the problem is associated with profisafe. Attached is my test project. Tried with D445-2 FW 4.4 and 4.5 Attachmenttest_compile_45.zip (117 Downloads) |
Last edited by: ggeihs03 at: 3/1/2017 2:45:02 PM |
|
3/1/2017 5:19 PM | |
Joined: 3/9/2015 Last visit: 9/19/2024 Posts: 17 Rating: (0) |
Hi Chistoph, I think the problem is easier to see on large projects. I increased the axis counts on the test project. Please compile the project a couple of times. You'll see it will compile in less than 5 seconds with no changes. Then simply add the profisafe telegram to D445->Sinamics_integrated->Drive_1. Recompile 2 or 3 times. You'll see that every compile goes triggers a HW config recompile, then resync of all addresses to the project. It takes 30-40 seconds to complete. No matter how many times I compile, this happens. If I remove the profisafe telegram and recompile a few times, the compile goes back to 5 seconds like I would expect. Hopefully you can see this on your end now,it's not just a simple incorrect message. Also, I'm not even looking at downloading now. This is purely just for compiling the offline project Attachmenttest_compile_45_take2parts.zip.001.zip (83 Downloads) |
Last edited by: ggeihs03 at: 3/1/2017 7:12:42 PM |
|
3/1/2017 5:19 PM | |
Joined: 3/9/2015 Last visit: 9/19/2024 Posts: 17 Rating: (0) |
Part 2 (remove.zip extension from this attachment and the previous one)
Attachmenttest_compile_45_take2parts.zip.002.zip (87 Downloads) |
Follow us on