3/28/2017 9:38 AM | |
Joined: 11/16/2012 Last visit: 9/21/2024 Posts: 307 Rating: (52) |
Okay, I have created an example project with four examples. The first two examples convert an INT value to a byte value and set it to outputs Q0.0 - Q0.7 if you work with 8 bits. The two other examples convert an INT value to a WORD value and set it to outputs Q0.0 - Q0.7 and Q1.0 if you work with 9 bits. The project was created with TIA V13 SP1 Update9. You can test it with PLCSIM, either with HMI or with watch table. AttachmentProject1.zip (63 Downloads) |
Last edited by: Min_Moderator at: 3/28/2017 3:27:46 PMUpload attachment |
|
Follow us on