3/23/2017 8:07 PM | |
Posts: 16 Rating: (0) |
No, i dont forgot change settings. In Set PG/PC interface i set my ethernet adapter TCP/IP. With MPI adapter all work, without dont. |
3/25/2017 10:13 PM | |
Posts: 16 Rating: (0) |
Good day! It was so similar to the solution, but it did not help I create new project and configureted network like in instruction in youre link 1 image - in hardware i add cpu and cp 2 image - in netpro i add pg/pc and add ethernet interface with ip 192.168.0.2 3 image - i added mpi interface to pg/pc with address 5 4 image - Conneted pg and controller to ethernet and mpi in netpro 5 image - ip address of cp is 192.168.0.3, mpi address is 3 6 image - mpi address of controller is 2 7 image - Compile and save in net pro - no errors Then i download hardware to CPU via mpi - no errors Then i change connection to TCP/IP and try download hardware - no errors Then i disconnected mpi connector 8-10 image - try download hardware to CPU and got error "Connection could not be established. The connection partner is not responding" "Unable to establish a connection to module CPU 315-2 DP (R0/S2)"
Whats wrong? Attachmentscreenshots.zip (356 Downloads) |
Last edited by: dieego6 at: 3/25/2017 10:14:27 PMLast edited by: Min_Moderator at: 3/27/2017 4:33:49 PMAdd attachment |
|
3/27/2017 6:22 PM | |
Posts: 54 Rating: (2) |
Hi Dieego, If you're connecting peer to peer do you have crossover cable? |
3/28/2017 4:52 AM | |
Posts: 16 Rating: (0) |
Hello Yanto, thanks, I'll try in 1-2 days, crimping pliers now do not have me |
4/2/2017 7:38 PM | |
Posts: 16 Rating: (0) |
Hello! Made the cable like this. See screenshot 1 This option also did not help everything remained unchanged. Here are screenshots from netpro -> properties cp343 -> Diagnostic. Look at the photo 7-8, I do not understand what kind of mistakes such
AttachmentScreenshots.zip (379 Downloads) |
Last edited by: Min_Moderator at: 4/3/2017 5:04:07 PMAdd attachment |
|
Follow us on