10/15/2009 9:08 AM | |
Posts: 378 Rating: (47) |
Hello to all, i don´t know much about this topic. But maybe these four other threads may help a little bit. Problem downloading (--- PANEL OP 7 ---). WinCC Flexible OP7. Connect OP7 <-> PC(USB) via converter RS232<>USB. CANNOT DOWNLOAD PROGRAM FROM LAPTOP TO OP3. Best regards bilao |
10/15/2009 7:09 PM | |
Posts: 13 Rating: (0) |
Is there any site where I can download a free version of Protool Panel? Or a full version, if it´s old, maybe it´s free... who knows! |
Follow us on