4/16/2017 3:00 PM | |
Joined: 11/7/2012 Last visit: 8/28/2023 Posts: 67 Rating: (0) |
Dear All, 1 - I have ring with around 39 IEDs 37 are 7SJ80 and 2 are 7UT613. There is a SNTP server tp sync all IEDs. The only IEDs are getting time sync are those two 7UT613 and the rest are showing NS ER on the front panel. attached you can find the EN-100 module home page for both synchronized (7UT613) and not synchronized (7SJ802) relays. 2 - I connect all IEDs in this ring one by one from one side forward and i can not ping the relay 18th relay on this row! is there any limitation on module to determine the number of IEDs on the ring cuz before i connected more than these on one ring and it was ok. Best Regards, AttachmentEn-100 home.zip (69 Downloads) |
Follow us on