5/25/2017 8:13 AM | |
Joined: 12/9/2010 Last visit: 10/8/2022 Posts: 623 Rating: (76) |
Hi Kbv, Can u share the manual u r referring? The module 6ES7331-1KF02-0AB0 does not have such setting. Resolution- As per my belief, resolution is used for RTD module. There are 2 possibilities like divide by 10 or divide by 100. For more accurate readings, u should use divide by 100. It is not related to no. of bits ADC. |
If you like the comment, rate it (right top) or thank it (left bottom). |
|
This contribution was helpful to1 thankful Users |
Follow us on