5/28/2017 10:57 AM | |
Joined: 7/16/2013 Last visit: 2/17/2023 Posts: 8 Rating: (0) |
Hello, Am facing a problem to upload backup from S7 314 C 2PN/DP PLC using software TIA Portal Version 11. Communication using MPI The backup which i have with me is not the final one so that there seeing changes in the online and offline programs. Attached images of software used for backup developed (TIA portal Update 2)and software installed in my laptop (TIA portal SP2 Update 2). The problem am facing is upload option is not at all enabling, though I am able to go online with the program . Please help... AttachmentSoftware details.pdf (185 Downloads) |
5/29/2017 10:17 AM | |
Joined: 5/12/2006 Last visit: 9/20/2024 Posts: 22365 Rating: (3011)
|
Hello, no there is no download available. Tia V11 is in status "discontinued" and only the latest SP2 Version is available for Download. I think the Upload is also not possible with a TIA V11 Install without SP2. From this FAQ (https://support.industry.siemens.com/cs/ww/en/view/97554052) it should be possible to Copy the blocks from the online PLC to a PLC in the project. Have you try this? Regards Chrisoph |
5/29/2017 11:02 AM | |
Joined: 7/16/2013 Last visit: 2/17/2023 Posts: 8 Rating: (0) |
Hi Mr. Chrisoph, Some what I managed to keep the software version both same. I will try the dat provided in the link and will update you. thanks for your kind support. With regards Sibin Earathe |
Last edited by: Sibin Earathe at: 5/29/2017 11:02:17 AM |
|
Follow us on