7/20/2017 1:08 PM | |
Joined: 6/24/2013 Last visit: 3/28/2024 Posts: 1582 Rating: (404)
|
Hi Each CPU has a FIXED number of Timers, Counters, M Bits, etc. it is not possible to increase these. Should You run out of timers it is possible to use: - IEC Timers which are SFBs and require instance data blocks (or as a multiple instance in calling FB) AttachmentON_Delay_Timer.pdf (52 Downloads) |
Follow us on