7/20/2017 12:32 PM | |
Joined: 11/29/2011 Last visit: 8/19/2024 Posts: 1359 Rating: (232) |
Hi, I am not sure what is your question here. Anyways any migration requires careful planning and preparation. Look at the From PROFIBUS DP to PROFINET IO. If you have further question please do not hesitate to ask! Just a note. Maybe you are better of solving the issues with the existing application. Profibus is very robust system if it is installed and commissioned properly it should not have issues. If you want to consider that option as well we also are here to help you with that. |
- What you read here, please check with manuals and your requirements. |
|
7/20/2017 1:04 PM | |
Posts: 54 Rating: (0) |
during 6 to 7 years we have cheked the solution related to bus |
This contribution was helpful to1 thankful Users |
Follow us on