11/21/2017 12:15 PM | |
Joined: 10/11/2006 Last visit: 4/26/2024 Posts: 5825 Rating: (789)
|
Dear Jerryvdk, in our opinion there is no Need for an stabilyzer at all. If you use the Active Line Module and Active Interface Module the voltage Rating in the catalogue is always with +-10%. So this Variation is within the tolerance. Furthermore with the use of an Active Line Module the DClink voltage of your drive System will remain stable during the voltage dips of the line supply. You can find the infomation on page 7/28 in catalogue D21.4: https://support.industry.siemens.com/cs/ww/en/view/109747019 |
With best regards, |
|
Follow us on