12/11/2017 11:56 PM | |
Joined: 10/7/2005 Last visit: 9/23/2024 Posts: 3022 Rating: (1054)
|
Hello RPalanzo "DO =" is a rather straightforward instruction and has nothing to do with the indirect addressing related "DO" command (apart from both having the name "DO" in it which easily causes confusion). While the the manual for your S5 CPU will have an explanation for the "DO =" Instruction in the Substitution section, the simple answer on what these instruction in your FB do is this: DO =OUTD // open DB 149 (same as "C DB 149" if DB149 wasn't an FB Parameter) |
Cheers |
|
Follow us on