2/15/2018 6:16 AM | |
Joined: 10/28/2014 Last visit: 4/17/2024 Posts: 63 Rating: (2) |
Hi I faced a problem with a S7400H system MLFB: 6ES7 414-5HM06-0AB0, FW: V 6.0.6. System was healthy and was running in redundant mode for several months. All of a sudden it was observed that rack0 CPU was in STOP mode. When i checked I found that a force was active on the CPU. After removing this force, I switched off and switched on rack0 and the system was healthy. Now I was going through the diagnostic buffer to find out what triggered this event, but I am unable to find the reason. I have attached part of the diagnostic buffer. How do I find out what triggered this problem? Thanks AttachmentDiag Buffer.txt (192 Downloads) |
2/22/2018 7:31 AM | |
Joined: 2/25/2011 Last visit: 9/6/2024 Posts: 67 Rating: (5) |
Dear Prassanna, Please attach full diagnosis. Thanks. |
2/22/2018 9:15 AM | |
Joined: 10/28/2014 Last visit: 4/17/2024 Posts: 63 Rating: (2) |
Hi Complete diagnostic buffer attached. Regards AttachmentCPU_Diag Buffer.txt (193 Downloads) |
3/5/2018 10:10 AM | |
Joined: 10/28/2014 Last visit: 4/17/2024 Posts: 63 Rating: (2) |
Dear Person Thanks for the input. I have raised a request with Siemens Support. |
Follow us on