9/7/2017 12:55 PM | |
Joined: 4/28/2015 Last visit: 9/9/2024 Posts: 3345 Rating: (379)
|
Hi community, I'm glad to share some specific node-red nodes for our SIMATIC IOT2000 with you. This "package" includes nodes for:
There are two different ways to include these nodes in yout IOT2000:
Here is a little example flow (User Button controls User LED):
Please feel free to use these nodes and give us some feedback! If you are facing any bugs, unexpected behavior or something else please post it in this thread or use github for it. Best regards! Attachmentnode-red-contrib-iot2000.zip (1039 Downloads) |
Last edited by: bergmanu at: 9/7/2017 1:35:31 PMLast edited by: bergmanu at: 9/8/2017 12:07:44 PMupdated attachment Last edited by: bergmanu at: 9/8/2017 12:09:43 PMNot working for IOT2050 support anymore from March 1st, 2024. |
|
This contribution was helpful to3 thankful Users |
9/8/2017 11:58 AM | |
Joined: 9/2/2013 Last visit: 11/6/2020 Posts: 48 Rating: (19) |
_ |
Last edited by: Ocean_ at: 9/6/2018 11:06:47 AM |
|
9/8/2017 12:08 PM | |
Joined: 4/28/2015 Last visit: 9/9/2024 Posts: 3345 Rating: (379)
|
Sorry for that. Now it is the latest version! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
2/12/2018 2:07 PM | |
Posts: 12 Rating: (1) |
Correct me if I'm wrong, but I can't see the nodes for the user button or user-LED? |
2/13/2018 12:30 PM | |
Joined: 4/28/2015 Last visit: 9/9/2024 Posts: 3345 Rating: (379)
|
Hi,
that's correct, you are right. In the first version the mentioned nodes were available. You can find some nodes for User Button and User LED here. Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
This contribution was helpful to1 thankful Users |
3/21/2018 8:34 AM | |
Joined: 2/6/2017 Last visit: 11/29/2023 Posts: 4 Rating: (1) |
Hi all, my topic concerns Adafruit PN532. In general my approach is "Extending the Node-RED capability of SIMATIC IOT2040. Implementing sensor node from scratch." If you’re using NodeJS to build a program for an IoT device like the SIMATIC IOT2040, then chances are you have, or will, run into a case where there is not a driver for the peripheral device that you’re trying to use. Please find the source in my git-hub repository under github.com/gull...b-rfid-nfc/wiki |
This contribution was helpful to3 thankful Users |
8/17/2018 1:25 PM | |
Posts: 8 Rating: (0) |
Dear Bergmanu, I can not access this node of IOT2000. what is the possible cause. please help me. kindly find attached file for your reference. |
Follow us on