5/25/2018 7:57 AM | |
Posts: 4 Rating: (0) |
Hi, im trying to connect PC and simatic s7-1200 cpu 121c ca/da/rly (1be40) firmware version - 4.1 tcon, trcv, tsend version v3.0 On assignment: 1. sent any message from the pc client to the server 2. received a reply 3. Send any message from the pc client to the server 4. received a reply aka messenger pc with simatic s7 this is my problem: From the side of the PC client. I enter a message to send to the server. I get a response from the server "helloworld" (correct msg). and the connection is lost by the error 0x80004005. from the server side. connection with the PC client, sending the message "helloworld" - has the status "done", but the message from the client is not received, the status of "recieved" is "busy". client code on c#
attached: AttachmentPictures.zip (44 Downloads) |
Last edited by: kipetilnik at: 5/25/2018 8:25:07 AMLast edited by: Jen_Moderator at: 5/25/2018 10:09:13 AMDeleted links and added all files as an attachment. |
|
5/25/2018 8:58 AM | |
Posts: 4 Rating: (0) |
Duris_I, I attached a zip with images. 1. The C # app tries to connect again. I'm sure. I checked. 2.
Probably yes. How to fix it? Attachmentreport.zip (48 Downloads) |
Follow us on