6/22/2018 8:23 PM | |
Posts: 1 Rating: (0) |
Hi,William_B "Option 3 does not work for the CPU1214." ''One problem .. what voltages can your encoder handle? If it is 5V, then you have to use a special signal board.'' Can you tell me the name of special signal board? I want use CPU1214 conecting incremental encoder with Line driver output type (5VDC) Thank! ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 7/2/2018 7:58:17 AMNew subject after splitting |
|
7/2/2018 6:10 PM | |
Joined: 7/7/2010 Last visit: 5/7/2024 Posts: 14688 Rating: (2351)
|
Drop in the signal board 6ES7-221-3AD30-0XB0 for 4xDI @ 5V. Then configure the inputs to accept your encoder signals.
|
science guy |
|
Follow us on