10/10/2018 9:42 AM | |
Posts: 1 Rating: (0) |
same scenario with the TS. is it possible to modify old project only by wincc 2008, without protool?\ EDIT: I am using wincc flex 2008 sp2 exactly, but everytime I opened the old project, its prompting that I have a missing software package which is PROTOOL. what should i do to get rid of this.? I just want to download the backup project (provided by the supplier) to new HMI panel. but this protool error is not allowing it ------------------------------------------------------------------------------------------ |
Last edited by: jefflunas1026 at: 10/10/2018 9:48:18 AMLast edited by: The Helping Hand at: 10/10/2018 2:35:23 PMNew subject after splitting |
|
Follow us on