3/16/2017 1:44 PM | |
Joined: 12/18/2014 Last visit: 9/25/2024 Posts: 33833 Rating: (4205) |
Which LOGO! 0BA8 do you have? Which software version do you have? Take a look at this link: Why can you not download any programs into your new LOGO! 8? |
3/16/2017 2:33 PM | |
Posts: 4 Rating: (0) |
Hi, |
Last edited by: Sinoscopis at: 3/16/2017 2:35:03 PM |
|
3/16/2017 2:36 PM | |
Joined: 12/18/2014 Last visit: 9/25/2024 Posts: 33833 Rating: (4205) |
Which LOGO! 0BA8 do you have? Which IP-Adresse has the PC? Which IP-Adresse has the LOGO!? Are the IP adresses static? |
3/16/2017 2:43 PM | |
Posts: 4 Rating: (0) |
Which LOGO! 0BA8 do you have? --> Standard LOGO 0BA8 Which IP-Adresse has the PC? --> 192.168.1.56 Which IP-Adresse has the LOGO!? --> 192.168.1.251 Are the IP adresses static? ----> yes |
Last edited by: Sinoscopis at: 3/16/2017 2:44:00 PM |
|
3/16/2017 2:45 PM | |
Joined: 12/18/2014 Last visit: 9/25/2024 Posts: 33833 Rating: (4205) |
If the problems only with Linux, take a look at this link: Bug-report: Java error in LOGOComfort V8.0 Linux Specially the post from the User WWE from 12/13/2014 1:37 AM. |
Follow us on