1/17/2019 3:30 PM | |
Joined: 9/27/2006 Last visit: 4/24/2024 Posts: 12257 Rating: (2665) |
Hello Med_Selmi; To start off my answer, here is a WinCC Professional interactive presentation that will give you many hints on what can be done with your SCADA soiftware: WinCC Professional presentation : https://www.siemens.be/cmc/upload/cms/docs/webinars/Simatic_WinCC_Professional_brochure_29052018.pdf Next, as usual, the manual I always recommend when starting something new with Siemens products. This will show you how Siemens recommends you create screens, communicate with your PLC, configure tags, logs, trends,and reports... WinCC Professional isnatalls a SQL server database for its internal logging of all screens, alarms, tags... There are export functions and optional packages you can use to send the data to outside applications. WinCC Professional v13 SP1 system manual: https://support.industry.siemens.com/cs/my/en/view/109096785 Open the section "WinCC Visualize Process" for detailed information on how to program the WinCC Professional application. Once the development of the application is finalized (or almost0, you will want to deploy the Runtime version so you can connect to the PLC, control the plant and collect data. For that you will need a WinCC RT Professional V13 license. The Catalogue ST80 (from 2016) contains the information on RT licenses). I have included the RT license numbers in the screenshot below; they are still valid, ask your Siemens rep for price and delivery.. Catalog ST80-2016 for WinCC RT Pro v13 SP1 license numbers (starting at page 3-18) https://www.automatyka.siemens.pl/docs/docs_ia/simatic-st80-stpc-complete-english-2016.pdf SIMATIC WinCC Runtime Professional is available as a software package with 128, 512, 2 048, 4 096, 8 192, 65 536, 102 400, 153 600 and 262 144 PowerTags. PowerTags are data points that are connected to controllers or other data sources via a WinCC Runtime Professional channel. Up to 32 alarms can be obtained from one data point. Moreover, internal tags without coupling are available for additional system performance. WinCC Runtime Professional also contains 500 archive tags. Additional archive licenses can be obtained for greater quantity structures. Hope this helps, Daniel Chartier Edit: Another ressource you can look at for your project: Demo project for WinCC Runtime Professional V13 SP1 https://support.industry.siemens.com/cs/ww/en/view/109478972 D.C. |
Last edited by: dchartier at: 1/17/2019 3:34:57 PMLast edited by: dchartier at: 1/17/2019 4:56:09 PM |
|
This contribution was helpful to2 thankful Users |
Follow us on