2/21/2019 1:44 PM | |
Posts: 2 Rating: (0) |
Hi All, I Have a project in which have Server Client architecture and AS-OS configuration. I have implemented Report system error function i got the result messages i wanted, but there is major issue when i compile OS station for message generation it gets overwrite in my manual generated texts in the text library. Please tell the proper way so that my manual generated text will not get effected while compiling OS Station to generate RSE Alarms. ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 2/22/2019 10:32:33 AMNew subject after splitting |
|
2/28/2019 6:54 AM | |
Posts: 2 Rating: (0) |
I'm using Simatic manager and WinCC 7.4 SP1. |
Follow us on