5/30/2018 11:40 AM | |
Joined: 4/28/2015 Last visit: 12/22/2019 Posts: 2 Rating: (0) |
Hi, I got a problem when installing WinCC 2008 SP5. If I double click Setup.exe to install, and select 'typical installation', then Microsoft SQL Server 2014 Express can be installed. However, if I first use /record parameter to generate a Ra_Auto.ini file (also choose typical installation), then install it with a command like like: start /wait "" "Z:\WinCC\2008SP5\Setup.exe" /Silent=D:\INI\Ra_Auto.ini Then SQL Server 2014 Express cannot be installed - it's simply not in the component list during the installation. The Ra_Auto.ini file has been attached. Is there a fix or workaround for this? Thanks! Regards, Bo AttachmentRa_Auto.ini.txt (193 Downloads) |
Last edited by: AutoGen_1070273 at: 5/30/2018 12:52:09 PM |
|
5/30/2018 11:59 AM | |
Joined: 5/12/2006 Last visit: 4/25/2024 Posts: 22227 Rating: (2980) |
Hello, what you mean with "cannot be installed"? Regards Christoph |
5/30/2018 12:02 PM | |
Joined: 4/28/2015 Last visit: 12/22/2019 Posts: 2 Rating: (0) |
No error message, SQL server express will simply not be in the component list when it's installed silently. |
3/18/2019 12:50 PM | |
Posts: 7 Rating: (0) |
Hello...anyone can help here ? Thanks ! |
Follow us on