3/23/2019 3:11 AM | |
Joined: 9/9/2015 Last visit: 4/11/2024 Posts: 727 Rating: (268) |
Dear Ahmed, May be you could check few things here. 1. The connection between the OS server to AS. Is it a project specific or station specific configuration? If station specific, make sure you merge the ethernet between them. 2. Check the connection in Netpro, make sure there is a s7 connection between OS server to AS. If you want to do OS Simulation from ES, make sure your have a s7 connection with the same name as OS server to AS in ES. Click to download selected station/download to selected and partner station. 3. full compile OS , make sure the connection settings correctly selected, Named connection or industrial ethernet. 4. after open up the OS, go to tag management, industrial ethernet/named connection, right click -> system parameter, make sure the connection is what you want. 5. start the runtime and check again. |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
3/23/2019 9:18 AM | |
Joined: 9/9/2015 Last visit: 4/11/2024 Posts: 727 Rating: (268) |
Dear Ahmed, I never faced this kind of issues before. Is it a software installation issue? Can you provide the below information: 1. Is your OS server a standalone IPC/ Workstation or running on Virtual machine? 2. Is this a fresh installation? Have you started WinCC runtime in this OS successfully before? 3. What type of connections are you using right now for the AS-OS connection? TCP/IP or ISO? Direct connection or through switches? Any possibilities to have IP conflicts with other stations? 4. Domain? Workgroup? 5. Antivirus installed? Firewall? |
Last edited by: JazTai at: 3/23/2019 9:18:51 AMLast edited by: JazTai at: 3/23/2019 9:19:23 AMLast edited by: JazTai at: 3/23/2019 9:20:02 AMPlease give me 5 stars Rating if my post is helpful for you. :) |
|
3/24/2019 4:20 AM | |
Joined: 9/9/2015 Last visit: 4/11/2024 Posts: 727 Rating: (268) |
Dear Ahmed, Did you change the server package from OS Single to OS MultiUser Project? Check the attachment. Attachment20190324_IMServerX.zip (252 Downloads) |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
This contribution was helpful to1 thankful Users |
3/24/2019 4:30 AM | |
Joined: 9/9/2015 Last visit: 4/11/2024 Posts: 727 Rating: (268) |
Dear Ahmed, At the same time, create a support request as well if the issue cant be resolved. Click the link here. |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
3/26/2019 2:29 AM | |
Joined: 9/9/2015 Last visit: 4/11/2024 Posts: 727 Rating: (268) |
Dear Ahmed, By default, multi project has that two ticks "Checked". But if it is not possible your case, then you would need to get Siemens Support already. |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
Follow us on