3/23/2019 8:48 PM | |
Joined: 12/18/2014 Last visit: 5/9/2024 Posts: 32993 Rating: (4078)
|
Hello abe708, at first welcome to the forum. But that is an unfavorable area and range. AttachmentCurrent_0BA8.Standard.zip (664 Downloads) |
This contribution was helpful to1 thankful Users |
3/24/2019 12:08 PM | |
Posts: 19 Rating: (0) |
Thank you for your answers, very helpful. I am using a Siemens Logo! 8 12/24 RCE - 6ED1052 - 1MD00-0BA8 with logo soft comfort V8 software. I attached sensor's datasheet and diagram connections, actually what it is supossed I need to do. It is just a first schematic. I need those sensors because I need to monitorize power consumption and power coming from photoltaic cells, just first steps. The idea is, working during whole development whith that coneections, pretending is a photoltaic installation and last steps work with a real one. Of course the sensor will be a bigger ones. But they will remain the same type, just increment current range. AttachmentSensor+Diagram.zip (581 Downloads) |
3/24/2019 2:33 PM | |
Joined: 2/22/2008 Last visit: 5/8/2024 Posts: 2698 Rating: (206) |
|
Follow us on