11/18/2013 10:43 AM | |
Joined: 4/29/2010 Last visit: 7/15/2024 Posts: 1557 Rating:
|
Hello alexandros, in the moment im not sure if you mean with "SCADA" just a pc-based device or the SCADA functionality.
With WinCC flexible you can project pc-based devices (PC-Runtime, PanelPCs,..) like in WinCC V7.x. The differenz ist just the functionality between WinCC flexible and WinCC V7.x.
This depends on the communication way you want to use. If you want to communicate via ethernet/ Profinet you don´t need a seperate card. If you want to communicate via MPI/Profibus you need a CP (if you use a normal pc).
Yes this is possible.
Maybe it would be better if you ask this two questions at the PLC/ STEP7 conferenz.
The advantage of the TIA Portal is that you can project the PLC and the HMI device all together in one software. The migration of the plc is also real easy because there is a tag converter wich can convert your datablocks/ tags,... directly into a TIA Portal project. TagConverter für WinCC (TIA Portal) With best regards |
This contribution was helpful to
1 thankful Users |
11/18/2013 10:54 AM | |
Posts: 25 Rating:
|
answer 1: wincc flex is diffent from scada u need to go with wincc 7.0 |
12/26/2017 8:05 PM | |
Joined: 6/19/2017 Last visit: 6/28/2024 Posts: 8176 Rating:
|
New question published by Gujaa is split to a separate thread with the subject SCADA system for profibus network. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on